2023-11-27 11:02 PM
Hi All,
I need to change parameter Minimum frequency "MIN_FREQUENCY_TH " by main.c
not chage in acim_vf_parameters.h
Please help me for advice.
BR,
Methee
Solved! Go to Solution.
2023-11-28 06:42 AM
#define MIN_FREQUENCY_TH 42
Maybe.
2023-11-28 06:38 AM
Hello @methee_c,
Some context maybe?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-28 06:42 AM
#define MIN_FREQUENCY_TH 42
Maybe.
2023-11-28 10:17 AM
Dear TDK,
Ok, now i can setting but can't set variable to float function need to constant only
BR,
Methee
2023-11-28 10:19 AM
Dear sarra.S,
Thanks you,
Ok, now i can setting in main.c but can't set variable to float function need to constant float only.
BR,
Methee