Hi All ,I need to change phase 120 degree to 90 degree in MotorControl Workbench 6.2.0 Can change in file mc_math.c?For use single phase motor 3 wire Please help me for advice. BR,METHEE
I can use it for Aruino ide but cube ide is very difficult to use. Can you make an inverter to sell if you are good at it? It didn't help me at all. It's better not to answer.
Dear Tesla DeLorean, I need to read data from eeprom for change information in parameters of MotorControl Workbench 6.2.0 project.But function parameters need to be const float or #define only.Please help advise. BR,Methee