cancel
Showing results for 
Search instead for 
Did you mean: 

How I can Define motor parameters...

oleg_sidorovich_1981
Associate II

How I can Define motor parameters if I do not find my board (steval spin3201) in Motor Profiler? Where is AN and anything??

1 ACCEPTED SOLUTION

Accepted Solutions
LYang
Associate II

:) You can measure the parameters. here is a construction video by ST:

 https://www.youtube.com/watch?v=XnGHpT96Ri4&list=PLnMKNibPkDnEgc7QwaabA5SKz5_4Mwz4e&index=2

View solution in original post

5 REPLIES 5
LYang
Associate II

:) You can measure the parameters. here is a construction video by ST:

 https://www.youtube.com/watch?v=XnGHpT96Ri4&list=PLnMKNibPkDnEgc7QwaabA5SKz5_4Mwz4e&index=2

Is there AN for that video?

Hi @oleg_sidorovich_1981​,

yes you can use the excel also for delta connection.

In both cases, the measurements is always made between two motor phases and the excel file translates the measures into an equivalent model that is unrelated to the actual motor phase connection.

If you feel a post has answered your question, please click "Accept as Solution"
Laurent Ca...
Lead II

Adding of STM32 Motor Control topic.

Best regards