2022-01-11 10:11 PM
2022-01-12 12:33 AM
The Embedded Partner Website of AVSystem says about Anjay LwM2M SDK:
Anjay is an LwM2M SDK that enables the LwM2M protocol on any hardware device. It features a completely internal implementation of CoAP and is able to run on any kind of platform. The product is released as an open-source and available at: https://github.com/AVSystem/Anjay.
Commercial options which include support and advanced features are also available as a terminator T800.
Probably only AVSystem will be able to help you and tailor the package to a specific target platform.
Regards
/Peter
2022-01-12 12:33 AM
The Embedded Partner Website of AVSystem says about Anjay LwM2M SDK:
Anjay is an LwM2M SDK that enables the LwM2M protocol on any hardware device. It features a completely internal implementation of CoAP and is able to run on any kind of platform. The product is released as an open-source and available at: https://github.com/AVSystem/Anjay.
Commercial options which include support and advanced features are also available as a terminator T800.
Probably only AVSystem will be able to help you and tailor the package to a specific target platform.
Regards
/Peter
2022-01-16 09:43 PM
Hi Peter,
Thanks you so much..
Please help us on below mention queries:-
Can you please share a link of terminator T800?
Can we interface LwM2M SDK with bare metal device or it required RTOS?
What are the minimum device configuration(Flash size, RAM size, GPIOs etc.) required for LwM2M SDK
Thanks
Vijendra
2022-01-16 11:40 PM
Please direct your questions to AVSystem, who will be sure to answer them to your satisfaction.
Regards
/Peter