cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F427 PB14 conflict with internal USB PHY

MBurg
Associate

Hi I am having the same problem as described in the old post down below.... is there a way to activate the link inside to see the fix? 

I am also using the external ULPI PHY, but when the USBD_Connect function executes, pin PB14 is lost. This is becasue the USBD_Connect function is enabling the internal PHY. I know there is a way to fix this but do not remember how. I needed to reinstall the whole environment so the fix was lost and now the code does not work since I need pin PB14 as a GPIO.

Here the post I am referring to:

https://community.st.com/t5/stm32-mcus-products/stm32f4xx-spi2-and-usb-hs-conflict/td-p/438246

Regards

 

Mark

1 REPLY 1
FBL
ST Employee

Hi @MBurg 

It is pointing to this thread

https://community.st.com/t5/stm32-mcus-products/stm32f4-i2s2-pin-af-multiplexer-issue-s/m-p/465934

If OTG_HS_GCCFG_PWRDWN is set (transceiver power down is deactivated) the DM/DP pins are driven by USB.

FBL_1-1739354545219.png

OTG_HS_GCCFG_PWRDWN is necessary to be set only when using the HS instance.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL