2020-04-19 4:30 AM
I'm using MCSDK_v5.4.3 but I don't know how can I convert additional ADC channel.
Below is ADC initialization code. added channel 9 and 10.
But I can't convert channel 9 and 10.
How can I convert ch.9 & 10.
Some sample code will very helpful to me.
Thanks
static void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
ADC_InjectionConfTypeDef sConfigInjected = {0};
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Common config
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV1;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.DataAlign = ADC_DATAALIGN_LEFT;
hadc1.Init.NbrOfConversion = 4;
hadc1.Init.DMAContinuousRequests = DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure Injected Channel
*/
sConfigInjected.InjectedChannel = ADC_CHANNEL_1;
sConfigInjected.InjectedRank = ADC_INJECTED_RANK_1;
sConfigInjected.InjectedSingleDiff = ADC_SINGLE_ENDED;
sConfigInjected.InjectedNbrOfConversion = 3;
sConfigInjected.InjectedSamplingTime = ADC_SAMPLETIME_19CYCLES_5;
sConfigInjected.ExternalTrigInjecConvEdge = ADC_EXTERNALTRIGINJECCONV_EDGE_RISING;
sConfigInjected.ExternalTrigInjecConv = ADC_EXTERNALTRIGINJECCONV_T1_TRGO;
sConfigInjected.AutoInjectedConv = DISABLE;
sConfigInjected.InjectedDiscontinuousConvMode = DISABLE;
sConfigInjected.QueueInjectedContext = ENABLE;
sConfigInjected.InjectedOffset = 0;
sConfigInjected.InjectedOffsetNumber = ADC_OFFSET_NONE;
if (HAL_ADCEx_InjectedConfigChannel(&hadc1, &sConfigInjected) != HAL_OK)
{
Error_Handler();
}
/** Configure Injected Channel
*/
sConfigInjected.InjectedChannel = ADC_CHANNEL_7;
sConfigInjected.InjectedRank = ADC_INJECTED_RANK_2;
if (HAL_ADCEx_InjectedConfigChannel(&hadc1, &sConfigInjected) != HAL_OK)
{
Error_Handler();
}
/** Configure Injected Channel
*/
sConfigInjected.InjectedChannel = ADC_CHANNEL_6;
sConfigInjected.InjectedRank = ADC_INJECTED_RANK_3;
if (HAL_ADCEx_InjectedConfigChannel(&hadc1, &sConfigInjected) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_2;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.SamplingTime = ADC_SAMPLETIME_61CYCLES_5;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_8;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC1_Init 2 */
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_9;
sConfig.Rank = ADC_REGULAR_RANK_3;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_10;
sConfig.Rank = ADC_REGULAR_RANK_4;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE END ADC1_Init 2 */
}
2020-04-19 6:26 AM
Are you saying this code converts channels 2 and 8 just fine but doesn't convert 9 and 10? Seems odd.
Make sure you're initializing the pins for channels 9/10.
2020-04-19 2:43 PM
I added initializing code for 9 & 10 and pin assignment also as below.
void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(hadc->Instance==ADC1)
{
__HAL_RCC_ADC1_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIO_InitStruct.Pin = M1_CURR_AMPL_W_Pin|M1_CURR_AMPL_V_Pin|M1_TEMPERATURE_Pin|ADC_9_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = M1_CURR_AMPL_U_Pin|M1_BUS_VOLTAGE_Pin|ADC_10_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
}
What I want to ask is how can I use below functions related regular conversion.
such as
uint8_t RCM_RegisterRegConv(RegConv_t * regConv);
uint8_t RCM_RegisterRegConv_WithCB (RegConv_t * regConv, RCM_exec_cb_t fctCB, void *data);
uint16_t RCM_ExecRegularConv (uint8_t handle);
bool RCM_RequestUserConv(uint8_t handle);
uint16_t RCM_GetUserConv(void);
void RCM_ExecUserConv (void);
RCM_UserConvState_t RCM_GetUserConvState(void);
Thanks
2020-06-23 4:43 AM
Hello,
Did you resolve the above issue??
if yes can you please let me know the solution?
Thank you.
2020-10-14 1:56 PM
Dear @Jace
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-10-26 2:24 AM
Dear @Jace
I guess you don't have to solve this problem anymore, therefore I consider this thread closed.
If not, feel free to reopen it by posting an answer.
Best regards
Laurent Ca...