2021-12-15 11:04 PM
I'm using TIM1 pwm generation ch1 ch1n & ch2 ch2n. My deadtime is set to 200. It's running at 100Hz and %50 duty cycle. I set the parameters as it should but nothing is working. My channel 1 & channel 2 settings are the same. Can someone help me to do it?
Thank you.
2021-12-31 07:17 AM
Dear @Sezer Özdemir
In STM32 Motor Control topic we do not deal with stepper motors control.
I move your question to the right topic (Motor Control HW).
Best regards