cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, i'm working with the EVSPIN32G4NH evaluation board to control a brushless motor. I cant find it on any ST Software. Does anyone know where i can find it? Thanks

MFlor.4
Associate
 
6 REPLIES 6
Javier1
Principal

https://www.st.com/content/st_com/en/ecosystems/stm32-motor-control-ecosystem.html

St provides a motor control workbench and a motor profiler, there is a chance your specific board is not supported, meaning that you need to add up all the details from EVSPIN32G4NH by hand, tedious but possible

we dont need to firmware by ourselves, lets talk

thing look good for you , the stm32g431 is supported in the FOC library

0693W00000SunOuQAJ.png 

we dont need to firmware by ourselves, lets talk

Hello Javier, Thanks for the quick response!

How do i add the STM32G431 to the library in th workbench ?

https://www.youtube.com/watch?v=MF7-tHG_qiQ

If your eval board is not supported by default you can click and write all parameters manually

0693W00000SuycxQAB.png

we dont need to firmware by ourselves, lets talk

0693W00000SuydvQAB.png

we dont need to firmware by ourselves, lets talk

That video shows the v5 SDK. What about the current (v6.0.0) SDK? The current SDK has a 'custom' option which only allows combining a handful of pre-defined evaluation boards. Once selecting the closest options there's no way to reconfigure most things (such as exact MCU, pin assignments, or even input voltage ratings).

Is the current SDK really only for toying with a few eval boards?