cancel
Showing results for 
Search instead for 
Did you mean: 

Generated .ioc file causes STM32CubeIde to throw an exception when it tries to open it

ABlak.1
Associate III

The attached ioc file causes STM32CubeIde to throw a nullptr excp.

It was generated by doing the following:

Open motor control wb 6.1.0

Follow the wizard to enter a v low inductance/resistance motor.

Select the B-G431B-ESC1 board

Generate the project

STM32CubeMX opens

"Generate Code"

Open STM32CubeIde

It opens and throws a NullPtrExcp

Please could someone at ST fix this defect?

1 ACCEPTED SOLUTION

Accepted Solutions
ABlak.1
Associate III

I downloaded the installer again and reinstalled it - it now works.

View solution in original post

2 REPLIES 2
ABlak.1
Associate III

I subsequently discovered this is the fault of the IDE and not specifically the ioc file. The IDE will not open any ioc file and in every case give a NullPtrExcp.

STM32CubeIDE

Version: 1.11.0

Build: 13638_20221122_1308 (UTC)

Windows 10.

ABlak.1
Associate III

I downloaded the installer again and reinstalled it - it now works.