2016-11-21 10:11 AM
Hello.
I want to use this SDK with encoder.I configured the encoder as the main sensor and programmed the EVB (I am using the P-NUCLEO-IHM001).The motor starts rotating, but then I turn the encoder wires off it continues to rotate at the right speed. Why?In this situation I'm pretty sure it would give a fault...I have the feeling that my encoder is not being used and the motor starts with sensorless and never enable encoder reading.Thank you. #encoder #sdk-4.32016-11-22 1:43 AM
Could it be something related to this?
2016-11-22 2:10 AM
2016-11-30 2:32 AM
Solved!
2016-12-08 12:46 AM
How solved?
2021-06-15 4:34 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards