Skip to main content
Associate
March 10, 2025
Question

STM32N6 VENC at higher resolutions

  • March 10, 2025
  • 19 replies
  • 6729 views

Hi,

We have STM32N6570-DK and are testing camera input, video encode and write to SD card

We have not been able to make the "VENC_SDCard_Appli" example work, the SD card just contains zeros.

The "VENC_SDCard_ThreadX" example does work however, resulting in an 800x480 video.

Are there any examples on encoding at 1080p resolution? Changing the encoder parameters and level results in memory allocation failures in EncAsicMemAlloc_V2.

Many thanks

 

19 replies

RomainR.
ST Employee
March 11, 2025

Hello @therealnerd2 

Can you provide details about the reading of the SD card for the VENC_SDCard_Appli demo? Did you follow all the recommendations in the Readme.html of this project below:

  • The configuration of OTP124 fuses VDDIO3_HSLV=1 I/O XSPIM_P2 High speed option enabled.
  • Have you signed and programmed the FSBL in external memory at address 0x7000 0000 and the Application at 0x7010 0000 by applying the correct header (STM32_SigningTool_CLI.exe)?
  • Are you viewing the image from the OV5640 camera on the LCD screen?
  • The re-reading of the SDCard must be done in raw mode as explained in the Readme.html in the section After execution.

Best regards

Romain,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
March 11, 2025

Hi,

We have been testing by running directly from the Cube IDE, and using Run and Debug. 

We have not flashed or programmed the OTP.

We can see the image on the LCD screen.

Command to read SD card attached.

Thanks.

 

Associate
March 11, 2025

If I step through the example, I can see that "encoder_prepare" is actually failing, but the error is not being checked.

The error comes from EWLmalloc, which is not able to allocate any memory.

Associate
March 11, 2025

I see this is https://github.com/STMicroelectronics/STM32CubeN6/issues/1. With that patch, the example now runs and the SDcard is now readable.

Associate
March 11, 2025

Can you please:

1) confirm if the patch in that issue is valid

2) explain how to increase the recording resolution to 1080p

ST Employee
March 12, 2025

Hello @therealnerd2 ,

Unfortunately, increasing the resolution to 1080p within VENC_SDCard_ThreadX requires a bit of work. The fact is that 1080p won't fit into the internal memory as in the original application. Camera and encoder buffer allocation requires some rework to be placed in external memory.

Best regards,

Daniel

Associate
March 12, 2025

Hi Daniel,

Thanks for the reply, this makes sense with what we are seeing.

Is such an example using external memory planned? It's a shame for a chip advertised as 1080p capable that we cannot easily prove this working and test power usage.

Many thanks.

ST Employee
March 13, 2025

Hi therealnerd2,

I understand your frustration.
We will strive to provide a 'ready-to-use' 1080p example in upcoming releases

Best regards,

Daniel

Associate
March 13, 2025

Great, thank you

Associate
March 13, 2025

Do you have any (estimated or actual) power consumption numbers for the device when doing a 1080p encode? Including the external memory ideally. 

Thanks

ST Employee
May 26, 2025
Associate III
May 27, 2025

Thank you @DanielS, that is a great reference!

Will this example soon be available in the STM32CubeN6 github?

Alternatively, where can the reference example be found that was used to take the power measurements?

Thank you in Advance.