2014-09-18 12:34 PM
Hi,
few days ago I downloaded the file ''STM32_FOC_SDK_4.0.0_Web_140625.exe'' from your homepage and wanted to try out the motion control on my custom board equiped with an STM32F407ZG device (either as single drive or dual drive). The driving IC is a Trinamic IC TMC603. Unfortunately I'm not able to test the TMC603, because the FOC 4.0 won't really work. I generated the dedicated header-files with the WorkBench and needed to adopt some pin settings (I use ADC3 instead of ADC1&2). After that I compiled everything without an error or warning (using Keil MDK-ARM). I did this with the provided example for MDK-ARM, but after MCboot() it seems that the microcontoller reset's itself everytime. The structures you need to provide the MCboot()-function are set with address 0x0 by firmware itself. If I force to run the application with internal RC-oscillator 16 MHz (instead of external 8 MHz) the address of this structures is somewhere around 0x200000xx in debugging mode over STLink (of course, the firmware won't work then because of the wrong timing settings). After this, I tried a completely new project and did it according the User Guide (Chapter 10.3) for STM32F4xx-devices. There are two libraries mentioned, which are precompiled but the MCApplication.a or .lib is not there. Even this library is not there, the MDK-ARM compiles (but now with warnings and few easy catched errors), but still not working. In the desciption I guess, some to-be-included files are missing, aren't they? I also tried to compile this library, but it seems I miss some ''confidential files'' as mentioned in the user manual. Is it possible to get this ''confidential files'' by subsrcibe a NDA ? So I would do that. Can you help me , please ? #stmcwb-foc-4.02014-09-22 2:37 AM
Ciao Marco
The problem that you get (reset of the micro) can be caused by a wrong setup of the PLL that set the CPU frequency. Please verify that the correct setting (according your hardware) is done the WB file that you use to configure the library (Control stage - MCU and Clock Frequency Selection) As usually I don't suggest to start with completely new ST MC Workbench new file but using one of the Example project like SDK40x-STM324xG-EVAL-MB459... and configure it acconding your system. Then you have to generate the params file and compile the FW using the IDE. The MCApplication.a or lib is no more used in the v4.0. It is part of the user project. Ciao Gigi2021-06-17 2:01 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards