cancel
Showing results for 
Search instead for 
Did you mean: 

EVSPIN958-SingleMotor firmware

de82
Associate

Hi, i'm using NUCLEO-F401RE product with EVSPIN958 expantion board connected to, for motor control.

I've connected this with STSPIN Studio 2.0, it's running correctly with EVSPIN958-SingleMotor firmware (i'm using DC brushed motor).

i'm just searching EVSPIN958-SingleMotor firmware code to use it as exemple.

I don't have found it on your site. Can you give me link to this information.

thanks.

1 REPLY 1
Cristiana SCARAMEL
ST Employee

Hello @de82 and welcome to the ST Community.

In general, for the STSPIN Studio environment we do not provide the code to drive the boards.

I can suggest you develop the code according to your application. You can use STM32CubeMX to set a timer for the PWM signal and possibly a timer for the current limiter.

 

If you feel a post has answered your question, please click "Accept as Solution"