2020-02-09 10:46 AM
How I can programming MCU (Example code with description, PID control, use STM32 Motor control SDK5.0, Motor control workbench and others)? Where is video example, AN?
2021-02-19 06:00 AM
The source code links no longer work ...
2021-02-19 06:19 AM
Hello @DavidePonte87 and welcome to the ST Community.
you can find the the firmware example of the EVALKIT-ROBOT-1 in the board page clicking on new Tab "Tools & Software".
Otherwise you can download it directly on the abovementioned STSW-ROBOT-1 page.
2021-02-19 06:24 AM
It makes me download the package version: 1.1, instead on the page it tells me about version: 2.0.0
it's normal ?
2021-02-19 06:31 AM
Thank you for reporting this misalignment of software versions between web and package.
In any case I confirm that the downloaded version is the last one released ;)
2021-06-15 12:52 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards