2019-11-27 12:29 AM
Hi, I'm a fans of STM32, i can write my code under linux well. But know, i wanna use adv motor control, i know ST has a MC SDK, but it for windows only?
i hope i can design my motor program on Linux.
Thank you !
Solved! Go to Solution.
2020-09-10 12:03 AM
Dear MMa.1893
Next release has been a little bit postponed and this feature will be probably integrated only in the next version.
Therefor, a full tools suite linux integration is not planned on the short term.
Best Regards
Laurent Ca...
2019-11-29 04:56 AM
Hello
yes we will 🙂
Unfortunately, it will not be ready soon :( - The target is Q2 2020 -
We are developing a new MotorControl Workbench from scratch that will be available for all platforms by construction. (Linux, MacOs, Windows).
In the meantime, a new MotorControl Monitor is also under construction and will be available for Linux too. It will be publicly available Q1 2020.
Regards
Cedric
2019-12-01 07:28 PM
wow!!
I am very excited. Hope the new tools will be more friends to linux command line tools chains..
2020-02-25 06:05 PM
any beta or preview version now? 😀
2020-06-03 01:42 AM
any update now?
2020-06-04 10:46 AM
We are working on it. now.. it should be for Q3 2020.
2020-07-23 10:52 PM
any update now? ^_^
2020-07-24 12:35 AM
Hello,
We are working on the new MC Workbench generation as planned. Unfortunately the very first version we are preparing now has some limitation and will work only with windows :(. But for sure we will solve this issue before the official release.
A question for you as well, which STM32 family are you using?
Thanks and best regards,
Claire
2020-07-31 12:00 AM
for now, STM32F3(stm32f303re) for adv bldc control
2020-09-09 12:28 AM
any update now?