cancel
Showing results for 
Search instead for 
Did you mean: 

DC-Motor Control Library for STM32 (VNH5019)

DBaum.3
Associate

Hello,

I would like to drive a simple DC motor with a STM32F446RE.

I use the VNH5019 as motor driver.

Everything works so far.

My only question now would be, is there a ready-to-use library or perhaps a way to embed the component into the software via STM32CubeMX?

Thank you very much

2 REPLIES 2

What, exactly, do you mean by "drive" here?

  • simple on/off?
  • speed control?
  • other ... ?

Have you looked on the Product Page for the VNH5019:

0693W00000QLsdSQAT.png 

DBaum.3
Associate

Hello Andrew, first of all thanks for your answer.

To describe it in more detail:

There is an EVAL board (STEVAL-VNH5019A) for the driver, which can be operated/tested with a Windows program.

The program offers various functions:

- Basic motor control (direction, start/stop, brake)

- PWM control

- Diagnostics

- ...

(see image)

I would now like to know if there is appropriate code or a library somewhere to do all of this on my processor

0693W00000QLtIQQA1.png