2024-12-01 08:43 PM
Hello,
I have successfully integrated the Bull Running Motor BR2804-1700kv with MCSDK(using the api whichever given by motor control library).
But Now, I have to run the motor with raw programming in stm32cubeide. I am using STM32F302R8 microcontroller and for motor driver IHM07M1 expansion board.
Why this process?
To understand how to set and control the parameters in stm32cubeide. Based on motor, how much the parameters in stm32cubeide will change.
Please help me to understand these concepts and give the response as soon as possible.
Regards,
Kamalesh
2025-01-07 05:59 AM
Hello @kamalskdy,
As already responded on this post, on ST side, we only provide support for MCSDK.