2021-05-14 12:38 AM
Project generation -> "UPDATE" does not update STM32 pin assignment.
AN5166 2.4.3: The preferred way to change pin assignment is obviously through the STM32 MC Workbench.
The only way to change pin assignment through STM32 MCSDK is to select "GENERATE"
2021-05-28 5:48 AM
Dear @Tore Kallevik
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and SW, CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, and so on)?
Best regards
Laurent Ca...
2021-05-30 11:53 PM
My project is with MCSDK 5.4.6, MCU STM32G474QE and STM32CubeMX 6.1.0