cancel
Showing results for 
Search instead for 
Did you mean: 

Can I use the TrueStudio for the P-NUCLEO-IHM001 board?

Jace
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
BTrem.1
Senior II

I have been able to build and run projects in the SDK_5.4.3 directory using the Keil Tool chain (MDK-ARM) though on some I needed to optimize size not time, to keep below the 32k limit on the Lite version.

View solution in original post

15 REPLIES 15
berendi
Principal

Yes. It has a STM32F302R8 MCU, any development environment can be used that supports it (or Cortex-M4 in general).

Ozone
Principal III

With the buy up of Atollic by ST, TrueStudio is more or less obsolete. I would not expect extensive support from ST.

Claire O.
ST Employee

Dear SPark.2,

I can confirm than the MCSDK is still ok with TrueStudio for yout board.

Thanks and best regards,

Claire

Jace
Associate II

Thank you for all your answers.

Jace
Associate II

Hi,

I bought a P-NUCLEO-IHM001 board and tried to generate c code as follow.

  1. Copied the "PotentiometerAdvance" folder to another location.
  2. Run the ST Motor Control Workbench (V5.4.3) and opened project "PotentiometerAdvance.stmcx"
  3. Project Generation
  4. Click "GENERATE" button
  5. RUN STM32Cube
  6. Selected TrueSTUDIO at Toolchain /IDE​ box
  7. GENERATE CODE and Opened project with Atollic TrueSTUDE IDE
  8. Selected "Build All" but I found next error

" fatal error: stm32f3xx_ll_bus.h: No such file or directory "

How can I fix it? Please guide me.

Thanks

Jace
Associate II

I solved the error but errors are continue..more and more.

Too many errors are generated. so I'll give up to use TrueSTUDIO.

I have the same hardware and went through the same steps described in the Project Potentiometer readme.txt file. I don't think its a TrueStudio Problem.

  1. Run ST MC Workbench 5.4.3
  2. Open potentiometer.stmcx and save to a new location.
  3. Select Generate--> build with ST32CubeIDE Tool chain (Update not given as option)
  4. Run ST32CubeMX and Generate Code
  5. Open project with IDE from STM32CubeMX.ioc file
  6. FW_F3 V1.11.0 is not latest, choose to migrate project
  7. Build All resulted in 9 errors, such as: fatal error: stm32f3xx_ll_bus.h: No such file or directory

I am trying to get local ST FAE help on this, very frustrated for 3 weeks now.

Claire O.
ST Employee

Dear Jace and BTrem.1,

Can you please check which version of CubeIDE or TrueStudio you are using?

We will check your problems,

Claire

I'm using SDK 5.4.3. I believe this is the latest available to date.