2020-02-13 07:03 PM
2020-03-05 01:58 PM
I have been able to build and run projects in the SDK_5.4.3 directory using the Keil Tool chain (MDK-ARM) though on some I needed to optimize size not time, to keep below the 32k limit on the Lite version.
2020-02-13 10:57 PM
Yes. It has a STM32F302R8 MCU, any development environment can be used that supports it (or Cortex-M4 in general).
2020-02-14 12:02 AM
With the buy up of Atollic by ST, TrueStudio is more or less obsolete. I would not expect extensive support from ST.
2020-02-14 02:07 AM
Dear SPark.2,
I can confirm than the MCSDK is still ok with TrueStudio for yout board.
Thanks and best regards,
Claire
2020-02-16 05:59 PM
Thank you for all your answers.
2020-02-16 08:03 PM
Hi,
I bought a P-NUCLEO-IHM001 board and tried to generate c code as follow.
" fatal error: stm32f3xx_ll_bus.h: No such file or directory "
How can I fix it? Please guide me.
Thanks
2020-02-16 10:20 PM
I solved the error but errors are continue..more and more.
Too many errors are generated. so I'll give up to use TrueSTUDIO.
2020-03-04 08:41 AM
I have the same hardware and went through the same steps described in the Project Potentiometer readme.txt file. I don't think its a TrueStudio Problem.
I am trying to get local ST FAE help on this, very frustrated for 3 weeks now.
2020-03-05 05:58 AM
Dear Jace and BTrem.1,
Can you please check which version of CubeIDE or TrueStudio you are using?
We will check your problems,
Claire
2020-03-05 06:10 AM
I'm using SDK 5.4.3. I believe this is the latest available to date.