cancel
Showing results for 
Search instead for 
Did you mean: 

What should I look for when changing the clock frequency in generated code with Motor Control Workbench?

HK
Associate II

I am working with ST-MotorControl Workbench. I generate the project according to 72 Mhz clock with WorkBench. I can't choose 56MHz through WorkBench. So, I re-generate project for 56 MHz with CUBEIDE. And than, I edit the code (picture). Is there any detail I need to consider when doing this editing process ?

0690X00000BwpYOQAZ.png

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Laurent Ca...
Lead II

Dear byHK

Do you have still this problem to solve?

Best regards

Laurent Ca...

HK
Associate II

I solved this problem. Thanks for answering!

Laurent Ca...
Lead II

Dear @HK​ 

I am happy for you.

Do not hesitate to share your solution with the STM32 Motor Control community.

Best regards

Laurent Ca...