2021-11-16 5:39 AM
I'm using MCSDK 5.4.5 in a high torque BLDC application.
DC bus voltage: 600V, motor power: 4kW, Hall sensors, current sensing with two insulated current sensors (7mOhm).
I had the effect that the motor power, returned by the API, switched to a negative value when increasing torque.
I have detected an overflow of the 32-bit variable wAux3 in the method PQD_CalcElMotorPower() in the file pqd_motorpower_measurement.c with my setup. If Iq is large enough and other factors such as PQD_CONVERSION_FACTOR are large as well, an overrun error occurs in the calculation.
By changing the order of the calculation, I was able to correct this effect.
I am now afraid that such an error can occur in other places in the code...
Question: is there a possibility in the MCSDK to adjust the scaling of the variables to fit on a high powert application?
2021-11-16 8:29 AM
Hello @CKlei.1,
Thank you for reporting this issue.
Right now there is no scaling mechanism in place in the SDK.
I will report this to our development team to add it in a futur version.
Regards
Cedric
2024-08-29 3:25 PM
I'm late to the party, but I was having the same problem.
Putting wAux3 divided by 10, before 6 times wAux3 worked for me!
Belated thank you to CKlei.1 for finding this nugget.