2020-09-16 05:16 AM
2020-09-17 12:05 AM
Hi @JBurg.2 welcome to the ST Community.
To start you could read the dedicated user manual UM2653 - Getting started with the EVALKIT-ROBOT-1
To make the kit operative you need:
Let me know if you managed to run the motor.
2020-09-17 05:53 AM
Hi, I have connected STS to pc via RS485-usb cable and supplied 36V. Motor moves to zero position. Now what communication software should I use ? Something from ST ?
2020-09-21 12:42 AM
Hi @JBurg.2
ST does not offer similar tool, you can find online some free communication software based on MODBUS protocol (e.g. QModBus, others are available).
Let me know if everything works.
2021-06-27 09:31 PM
Adding of STM32 Motor Control topic.
Best regards.