JBurg.2
Associate
since
2020-09-14
2023-06-14
User statistics
2
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About JBurg.2
Options
Report User
User Activity
Posts
Replies
Bought a EVALKIT-ROBOT-1 with driver STSPIN32 and Maxon servo motor . I have no idea what else I need to make motor work. Motor Profiler dont list this driver. It connects with modbus to pc. Can I just type c++ code and make it work?
2020-09-16
Re: Bought a EVALKIT-ROBOT-1 with driver STSPIN32 and Maxon servo motor . I have no idea what else I need to make motor work. Motor Profiler dont list this driver. It connects with modbus to pc. Can I just type c++ code and make it work?
2020-09-17
Hi, I have connected STS to pc via RS485-usb cable and supplied 36V. Motor moves to zero position. Now what communication software should I use ? Something from ST ?