cancel
Showing results for 
Search instead for 
Did you mean: 

BLDC Motor Control in Torque Mode

dsystem
Associate II
Posted on April 12, 2018 at 12:24

I am working on project using STEVAL-SPIN3201 board with SDK4.3.0.

I am able to control in speed mode. 

I want to know procedure to Read Present torque, How to set Torque value and How to Relate it with Current.

Secondly when I use commands related to Torque, like:

Run_Torque = MCI_GetTorque(oMCI[0]); 

I get error

error:  &sharp167: argument of type 'CMCI' is incompatible with parameter of type 'CSTC'

Also I want to Change mode during run time. How to do it ??

Regards

Vimal Amin

#bldc-torque-mode
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards