2017-10-04 4:09 AM
Hi!
I am using FOC 4.3 with a NovoMotec 1 pole BLDC motor. I can not start the motor at all. The PWM -s are working, and the motor vibrates, but the PWM signals have bad timing, thus braking the motor all the time.
Does anyone know, what parameters can I adjust, to tune the Hall-sensor timing?
Additional question:
What are these parameters?
2021-06-27 10:48 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards