STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1740 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4888 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9585 Views
  • 5 replies
  • 3 kudos

Connection Failed SPIN3204

Hi,I have a STEVAL-SPIN3204 board. I have opened the 6step_steval_spin3204 project on the ST motor control workbench, generated the code withe the following parameters using UPDATE button:STM32CubeMx: 6.5.0Target Toolchain: Keil MDK-ARM V5Firmware Pa...

dbuso.11 by Associate II
  • 617 Views
  • 0 replies
  • 0 kudos

Why cannot I get desirable PWM output?

Hi there,I'am using STEVAL-SPIN3201 evaluation board. I've reset PA11 for overcurrent output signal visible only to MCU and set PF6 and PF7 for overcurrent protection limit. Also, I've configured TIM1 channel 1 PA8 pin to center aligned pwm mode. Whe...

finding the cause for MOSFET burning STM32G431

Hey @ allthe setup: custom motor control PCBmicrocontroller: STM32G431CBU6gate-driver: UCC2721, 15Vthree shunt lowside current sense 150 µOhmOPAMP MAXIM MAX40056 20V/Vinverter stage: 24x IRF7759 (4 parallel)gate resistor 4,7 Ohmgate-source resistor 2...

0693W00000WHyo3QAD.png 0693W00000WHyuaQAD.png 0693W00000WHyv4QAD.png
ALedi.1 by Associate III
  • 1512 Views
  • 0 replies
  • 0 kudos

How to change polling of the Motor Pilot plot ?

Hello,In the documentation STM32 MC Motor Pilot :« Viewing and plotting registers with low-speed plotting.With this method of plot, any register can be plot but at low rate (polling every 200 ms by default) »I want to use the Motor Pilot plot (low sp...

Agran.1 by Associate II
  • 1322 Views
  • 1 replies
  • 0 kudos

When PWM duty changes?

Hello,I control BLDC motor.Control the speed of the motor by changing the TIM->CCR.​I have a question while setting the time to change the value of CCR.If I change the value of CCR while I'm sending out PWM, will the Duty ratio change in the next cyc...

hjuns by Associate III
  • 1203 Views
  • 1 replies
  • 0 kudos

Resolved! [Bug report MCDSK 6.0.0] Missing files when generating code with "Copy only the necessary files" option

The MC Workbench tool generate a CubeMX 6.5.0 project, that in turns generate C code.Actual behaviorWhen I select in this CubeMX project Project Manager > Code Generator > Copy only the necessary files, the generated IAR 8.0 project does not compile ...