cancel
Showing results for 
Search instead for 
Did you mean: 

BLDC and Motor Profiler

cristhianchr
Associate II

Hi! I am developing a project with a BLDC motor. It is possible to use Motor Profiler with a BLDC motor. The options only allow me to use Motor Profiler with PMSM.

 

Thank you in advance!

1 REPLY 1
GMA
ST Employee

Hello,

You can profile the motor with MCSDK profiler tool.
The Workbench selected motor at profiler project generation step is not taken into account for the profiling itself.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA