2022-09-22 7:44 AM
Hello,
I am new to the ST motor control workbench.
Already did the the initial steps of reading UM3027 and using the profiler and MC-SDK v6.0 Workbench GUI to generate a CubeIDE project.
The generated project only does initialization. The while loop is empty.
Now I want to test reading the hall sensors and doing basic velocity control (and later position control) using the code API.
I am struggling to find the appropriate functions.
Can someone point me to the API documentation (list of functions available) ?
Thanks!
2022-11-14 3:27 PM
I am new to ST and their associated tools. I am not able to pick the B-G431B-esc1 in Motor controller workbench 6.0. It is not in the list controllers. there is a of box called Power and a box called control but not one for inverter which is where this board resides in motor controller Workbench 5.4.8.
So I am very curious how you have been able to use this?
Does Motor Controller Workbench 6.0 actually support B-G431B-esc1?
Why is this post gone so long without a reply from ST?
2023-09-05 5:13 AM
Hello @DGuim.1 and @A1bucker
We would like to sincerely apologize for the delay in replying to your post.
If your point is still pertinent, B-G431B-esc1 is supported in MCSDK 6.1.2 and should also be supported in the upcoming MCSDK 6.2.0, you will find all the necessary documentation at this link:
Documentation post