cancel
Showing results for 
Search instead for 
Did you mean: 

B-G431B-ESC1 software and motor parameters Rs, Inductance.

SRedd.5
Senior III

When i refer the source code of the B-G431B-ESC1 board, i do not see the code check for series resistance, inductance of the motor. Is the source code independent of the series and inductance of the motor? For example

/***************** MOTOR ELECTRICAL PARAMETERS ******************************/

#define RS           0.35 /* Stator resistance , ohm*/

#define LS           0.0006 /* Stator inductance, H

But i do not see these parameters used anywhere in the program. Is my understanding correct?

1 ACCEPTED SOLUTION

Accepted Solutions
JKong.3
Associate III

it's in Inc/pmsm_motor_parameters.h

View solution in original post

1 REPLY 1
JKong.3
Associate III

it's in Inc/pmsm_motor_parameters.h