2022-01-26 05:50 PM
I'm looking at different alternatives for PLCs and I would love to use STM32 as one, but it seems like the boards that STM sells are all eval boards or individual boards. I'm lookin for a completed product that has stepper motor control and GPIO. Is there anything out there like that?
2022-01-27 01:58 AM
STMicroelectronics is not a supplier of PLCs, but does supply components that can be used to build a PLC, for example. The boards are intended exclusively for the evaluation of the respective component and for the development of own products, as can also be read in the Open Reference Material License Agreements, e.g. here, and the Terms of Use.
But I am sure you will find a supplier of such a PLC based on an STM32.
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2022-01-27 03:58 PM
Where would I find a provider? If I google it nothing useful comes up, and I can't find any partners in the partner finder that say they make a PLC.