‎2022-03-03 08:40 AM
I've been trying to develop a C++ application which uses the C based MC SDK (would really be nice if STM would provide a supported wrapper).
I'm getting:
arm-none-eabi-g++ -o "nucleo_demo_y4.elf" @"objects.list" -mcpu=cortex-m4 -T"C:\Users\dustin\repos\wheel\nucleo_demo_y4\STM32CubeIDE\STM32F302R8TX_FLASH.ld" --specs=nosys.specs -Wl,-Map="nucleo_demo_y4.map" -Wl,--cref -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group
c:\st\stm32cubeide_1.8.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: ./Application/User/wheel_ctrl.o: in function `Wheel::WheelCtrl::GetParam(Driver::CANDataPacket*)':
C:/Users/dustin/repos/wheel/nucleo_demo_y4/STM32CubeIDE/Debug/../Application/User/wheel_ctrl.cpp:62: undefined reference to `RI_GetRegCommandParser(MCP_Handle_t*, unsigned short)'
collect2.exe: error: ld returned 1 exit status
Searching the .map file I can see the issue, which seems to be a compatibility problem with the way C generates its references and the way C++ does.
.text.RI_GetRegCommandParser
0x0000000008003cc0 0x8bc ./Application/User/register_interface.o
0x0000000008003cc0 RI_GetRegCommandParser
...
RI_GetRegCommandParser ./Application/User/register_interface.o
./Middlewares/MotorControl/mcp.o
RI_GetRegCommandParser(MCP_Handle_t*, unsigned short) ./Application/User/wheel_ctrl.o
As you can see my wheel_ctrl.o references RI_GetRegCommandParser with the whole function call where as C only specifies the name. What's odd is other calls to MCI_ functions like MCI_ExecSpeedRamp and MCI_StartMotor seem to be referenced the same... I've tried a number of ways of calling RI_GetRegCommandParser and they call get the full (MCP_Handle_t*, unsigned short) reference in the .map.
Here's how I'm using it (last of various methods of storing MCP_Handle_t)
MCP_Handle_t* param = new MCP_Handle_t
{
.pTransportLayer = nullptr,
.rxBuffer = msg->data,
.txBuffer = msg->data + MCP_ID_SIZE,
.rxLength = MCP_ID_SIZE,
.txLength = 0,
};
uint8_t retval = MCP_CMD_OK;
retval = RI_GetRegCommandParser(param, MCP_FREE_TX_SPACE);
Really appreciate any advice to try, this is my final error and really trying to get this done so I can test on hardware.
Solved! Go to Solution.
‎2022-03-03 09:53 AM
Problem solved! 😅
The register_interface.h didn't have:
#ifdef __cplusplus
extern "C" {
#endif /* __cplusplus */
...
#ifdef __cplusplus
}
#endif /* __cpluplus */
Ooops! I thought I checked all the headers!
‎2022-03-03 09:53 AM
Problem solved! 😅
The register_interface.h didn't have:
#ifdef __cplusplus
extern "C" {
#endif /* __cplusplus */
...
#ifdef __cplusplus
}
#endif /* __cpluplus */
Ooops! I thought I checked all the headers!
‎2022-03-03 10:42 AM
Please mark the solution: