STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1713 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4867 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9536 Views
  • 5 replies
  • 3 kudos

Doing 6-step using FOC algorithm

Hello,I've generated a functional FOC project, with speed encoder. I also have Hall sensors wired (only used for my 6-step mode).I'd like to implement a basic 6-step control mode in this project.The FOC code allows me to set (eg. during the encoder a...

STM32 Motor Control SDK FreeRTOS

In STM32 MC SDK Workbench, is it necessary for me to tick the choice "Enable MC IRQ to use FreeRTOS Functions" when I enable FreeRTOS? In what circumstances should I tick this option? What happens when I don't enable this functionality? Anybody else ...

Screenshot 2023-09-19 144115.png
TimRocky by Associate
  • 2123 Views
  • 1 replies
  • 0 kudos

Resolved! project generation issue

when i generate the  project in the mcsdk then it continue showing like this .i have wait long time its still showing same, what i am doing wroing ?

RanjeetSingh_0-1695123871474.png

Resolved! Not able to go beyond certain Torque (10NM)

I am using the custom board based on B-G431B-ESC1 and the same software, but i am struggling to go beyond 10NM torque i am really not able to understand the root cause of the issue. One observation is the Valpha and VBeta is going beyond 28000. Is th...

SRedd.5 by Senior III
  • 1343 Views
  • 1 replies
  • 0 kudos
ppota.1 by Associate
  • 1483 Views
  • 1 replies
  • 0 kudos

Resolved! want to check with CTM007V1 instead of CTM006V1

Hi all,I'm currently having CTM007V1 driver board for motor control application. the control board is stm302r8 MCU and the driver board is STEVAL - TTM001V1. can i use modify the CTM006V1 firmware and replace it with CTM007V1 firmware? Regards, Siva.