cancel
Showing results for 
Search instead for 
Did you mean: 

Adding STM32G473 Support to STM Motor Control SDK 5.4.8

hwteam
Associate

Hello,
I am currently working with the STM Motor Control SDK (version 5.4.8) and noticed that it only supports STM32G474, while my project requires using the STM32G473 microcontroller.

Is there an option to add STM32G473 as a new package to the SDK? If yes, could you guide me through the process or provide relevant resources?

Any insights, suggestions, or references would be greatly appreciated.

0 REPLIES 0