cancel
Showing results for 
Search instead for 
Did you mean: 

ACIM and NUCLEO-G431RB

Gabe
Associate

Hello Everyone,  

I'm trying to perform a command for ACIM, I created the code generated by MotorControl Workbench 6.2.1 without any problems and I'm using the NUCLEO-G431RB kit..

I'm analyzing the PWM signals on the oscilloscope together with a filter to see the sinusoids, so far it works correctly...

What I noticed is that the V/F algorithm does not work as desired when I use the commands in the mc_api.c file

Basically I see that only the frequency is changed, not the voltage...

But when I start from MC Workbench it works, only for initial voltage...

Basically I can't change the voltage, only the frequency... what am I doing wrong, could you provide me with the correct function to solve this?

Thanks

 

Doubt.png

 

0 REPLIES 0