2020-02-14 8:19 PM
Hi all,
i am working on AC servo motor driver. at initial i just want to rotate the motor at different speeds. i am driving 6 mosfet shown in image by using stm32f030r8t6's TIM1. here is the programme that i have made. by this program motor runs but i am not able to change the speed of motor.
note : i am not considering encoder here as i just want to first rotate motor at different speed by changing in the programme.@Community member
2020-09-11 2:23 AM
Dear sanju
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-09-11 2:42 AM
Yes still I have this problem.
2020-10-16 12:26 AM
Dear @sanju
Could you give more details to the STM32 Community about the material you use (HW and SW, tools and versions, board(s), motor(s) and so on)?
And more especially did you use MC tools (MC_suite, MC-Motor Profile, MC-SDK, MC-workbench, and so on)?
Best regards
Laurent Ca...
2020-10-26 1:34 AM
Dear @sanju
As you do not answer, I guess you don't have to solve this problem anymore, therefore I consider this thread closed.
If not, feel free to reopen it by posting a new answer.
Best regards
Laurent Ca...