cancel
Showing results for 
Search instead for 
Did you mean: 

Absence of "Start Hall Profiling" in Motor Pilot 6.4.1 Profiler

pelino
Associate III

I am using Motor Pilot 6.4.1 Profiler and noticed that there is no "Start Hall Profiling" option available.

Could you please confirm if this feature has been removed or if it is located elsewhere?

pelino_0-1768348283887.png

Best regards

Pelino

 

1 ACCEPTED SOLUTION

Accepted Solutions
GMA
ST Employee

Hello @pelino,

Feature is available enabling HALL sensor as auxiliary sensor.
Refer to 5. Hall sensor profiling with the Motor Profiler tool chapter of the Motor Profiler Application Note document available through "Workbench tool">About>Documentations>Documentation>"User manual" tab.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

2 REPLIES 2
STuser2
Senior III

The Start Hall Profiling option comes when the profiling (Start Profile) is successful. 

GMA
ST Employee

Hello @pelino,

Feature is available enabling HALL sensor as auxiliary sensor.
Refer to 5. Hall sensor profiling with the Motor Profiler tool chapter of the Motor Profiler Application Note document available through "Workbench tool">About>Documentations>Documentation>"User manual" tab.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA