cancel
Showing results for 
Search instead for 
Did you mean: 

About project generation at "st motor control workbench"

駿茂手木.1
Associate

I would like to ask a question about "st motor control workbench".

When I generate the sample project of STEVAL-SPIN3204, I get the following error.

I want to solve this error.

If anyone has been in the same situation and was able to solve it, please help me.0693W00000QKG3eQAH.png

2 REPLIES 2
Dane._.T
Associate II

I got it to generate on MotorControl Workbench 5.4.8 with the following settings:

STM32CubeMX - 6.5.0

Target Toolchain - ST STM32CubeIDE

Firmware Package Version - STM32 FW V1.11.3

You also may have clicked the "Generate" button. Sample projects usually require clicking the "Update" button to work properly.

駿茂手木.1
Associate

0693W00000QKMfUQAX.pngThanks for replying. I am working in this environment right now.

STM32CubeMX - 6.6.0

Target Toolchain - ST STM32CubeIDE

Firmware Package Version - STM32 FW V1.11.3

I have successfully generated the code with the "update" button. However, I am unable to build the project.

I was able to build when I hit the "generation" button to generate code for a different board, but were you able to build yours?