2023-11-21 12:04 AM
Hi,
I have an STM32H573I-DK Discovery kit with me. I wanted to try out Edge AI applications on it, and was checking out the STM32Cube.AI Developer Cloud. When I reached the "Generate" section and browsed through the listed boards, I could not find any of the STM32H5 series MCUs listed. Is it because they are not supported?
Will I be able to use it if I use X-Cube-AI with CubeMX?
Solved! Go to Solution.
2023-11-21 12:40 AM
Hello @georgethomas
STM32H5 serie is not available yet on STM32Cube.AI Developer Cloud. It will be available in a next release.
If you want to work on STM32H573I-DK, you can start today on STM32CubeMX with X-CUBE-AI, it is supported.
Best regards,
Yanis
2023-11-21 12:40 AM
Hello @georgethomas
STM32H5 serie is not available yet on STM32Cube.AI Developer Cloud. It will be available in a next release.
If you want to work on STM32H573I-DK, you can start today on STM32CubeMX with X-CUBE-AI, it is supported.
Best regards,
Yanis
2023-11-21 12:42 AM
Alright, thank you :thumbs_up: