2015-08-05 12:53 PM
Hi,
(Sorry, translated by ...)
I have questions about which I am not find anything on the Internet.I have with examples and advice from the web a virtual com port for STM32LXX MD and HD devices created.
This works in your own applications under XP, Win7, Win 8, Win 8.1 as x32 and x86 machines with no problems. Send and receive, hot-plug, data rates up to 400 kB, there are no problems.
Windows side, I have the STM drivers 1.3.1 or 1.4.0 can use as trouble-free.
My Windows programs use GetDefaultCommConfig, CreateFile, SetCommState, GetCommState, WaitForSingleObject ... ... to manage the ComPorts. Other virtual com ports (eg CP210 devices) I can speak without problems with my software under Windows 10.
Under Windows 10 but does my created virtual Com port no longer!
The STM drivers can be good and error-free installation, the status code is OK = 0x0. Connected devices are immediately recognized and duly incorporated as a COM device COMXX. Everything looks good.
I can sign by the PC to send and receive them on the microcontroller via USB.
But, mark returned but do not come to the PC. No character comes back. Windows 10 only.
Has anyone had similar experiences of you?
Have any of you STM CDC Examples under Windows 10 brought to work?
Is a modified Windows 10 functionality to blame? (A note would be that eg FTDI on 28/07/2015 new drivers brought out.)
If STM implement new drivers for Windows 10?
Could my PC (and other virtual machines) be guilty despite an OK from the driver?
If other STM-CDC examples run under Windows 10, where I would have to begin to repair?
Thanks for any information I can get.
Best regards
Gerald Loh
#vcp #stm32 #usb #cdc #windows102015-08-10 11:26 AM
I have
solved the problem
for the time being
.
Under
Windows
10
(
and
only on Windows
10
)
suggests
to me
the PC side
the
Microsoft
function
ReadFile
fails
, it returns
the
permanent
''
GetLastWin32Error
''
''
ErrorIOPending
''
.
In fact,
does this
function
until
this
error message
.
The
sign
,
which
you
must
read aloud
ClearCommError
/
ComStat.InQue
(
ie
the
ReadCount
)
are
,
nevertheless
transferred successfully
despite the error message
in
the buffer
.
If
I ignore
the error message
,
I can
again
communicate
via
VCP
.
Uses the
class
Serial Port
(
.NET
System.IO.Ports
)
one seems
to be working
to communicate
well
.
(
This
I have tested
only
a few
bytes
)
.
Whether
the fault
the
''
standard
device classes
''
or
''
my
controller
functionality
''
is now
attributed to
the future
will probably
show
...
2015-11-07 1:49 PM
Hi Gerald!
How exactly did you solve this problem. because I have the same problem?Best regards, Robert2016-05-11 11:24 PM
Hello.. Gerald
We have the similar problem in Win10.When we disconnected the usb port, Windows CPU load goes up suddenly. and there are so many errors. We want to know how did ignore the error? Could you be more specific? or Would you mind sharing your code?2016-05-12 12:57 AM
The original post is more than 8 month old, and obviously auto-translated into english.
That would suggest that the OP is not monitoring the forum.>We want to know how did ignore the error? The function/method names he mentioned are part of the Win API, so it seems he was speaking about a Windows based tool using the VCP. Trying to interpret the auto-translated text, he suggests to clear the COM error withClearCommError
(), and read out the received character(s) anyway. That would not be helpful on Desktop /GUI level.