STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Default S/W Listing for STM32F7508-DK

The S/W included in this Discovery Kit is nice as a demo, but as expected, I would like to tailor it to my application. I have not found any listing for the entire S/W included in the DK, perhaps because it is proprietary and the demo is basically an...

DRobe.4 by Senior
  • 1554 Views
  • 3 replies
  • 0 kudos

USB CDC to DAC

Hi, I am succesfully sending the data through libusb to the changed CDC example. But i need to use the CDC_Receive_FS function to send the data from USB buffer to DAC with DMA. So USB transfer speed is faster than the speed Timer triggers the DAC-DM...

B??el by Associate II
  • 834 Views
  • 0 replies
  • 0 kudos

STM32 USB HAL TxFIFO Error

Posted on February 23, 2018 at 18:29This is a reposting of https://community.st.com/thread/45731-stm32f7-hal-ll-driver-bug?sr=inbox with a more descriptive name. I am using the USB FS device with the CDC class. I used STM32CubeMX V4.23.0 with the ST...

MDS by Associate III
  • 3990 Views
  • 7 replies
  • 0 kudos

STM32 USB port connection problem.

Hello all,I have problem with my USB application. I am using Atollic and CubeMx on Windows 10 system. The USB connection gets disconnected when I enter debug mode for STM32F446RE nucleo board. Then I tried using Nucleo H743ZI board, the board is dete...

urath by Associate III
  • 1576 Views
  • 3 replies
  • 0 kudos

STM32L4 CDC handler

Hi all,I am now experiencing problems with USB stuck.I am using an STM32L433CC MCU.There are two blocks in Flash, one is Bootloader and the other is API code.Mainly at the beginning I entered the bootloader and can clearly know that USB can work.Also...

0690X000008w1EzQAI.jpg 0690X000008w1F4QAI.jpg 0690X000008w1F9QAI.jpg 0690X000008w1FEQAY.png
1123 by Associate II
  • 710 Views
  • 0 replies
  • 0 kudos

Resolved! RTC IRQ STM32L476

With the STM32 in stop mode 2, is it possible to use the RTC as a additional low power timer?I mean to trig IRQ periodically.I tried the PWR_STANDBY_RTC STM32Cube_FW_L4_V1.14.0 example for STM32L476 and the code never stop at the breakpoint in functi...

Mich1 by Associate III
  • 1581 Views
  • 3 replies
  • 0 kudos