2020-11-10 10:13 AM
2020-11-10 11:02 AM
Hello @MKulp.1 ,
Welcome to the STM32 Community =)
Which Cube package, please ?
Imen
2020-11-10 11:07 AM
STM32Cube_FW_L5_V1.2.0 has it. Removed from my repository on STM32Cube_FW_L5_V1.3.0. My customer discovered what appears to be a bug, and wondering if reason for removal. Should I (as the Avnet FAE) direct customer away from this example?
Thanks,
Mike
2020-11-11 1:23 AM
I'am checking it internally and I will come back to you with details.
Imen
2020-11-12 7:15 AM
No, you can't use this application, as the FreeRTOS 10.2.1 does not support LowPower mode for the CM33.
The Tickless IDLE is only supported in the 10.3.1 release
https://github.com/FreeRTOS/FreeRTOS-Kernel/commit/177e79fc79b62e8301f85ed19633c8aef5ef708d
Please select the post as a "Best Answer" if it answered your question, so that this thread will marked as closed.
Imen