2019-07-02 3:26 AM
I am designing a data logger with STM32L4.
I want to transfer the data stored in STM32L4 to a Windows 10 PC by USB CDC.
USB full speed transfer is 12Mbps and transfer overhead at CDC overhead, so I think STM32L4 can be about 4 to 6Mbps.
Who is know transfer speed can be?
2019-07-02 3:48 AM
I think your estimations are accurate; I remember approaching about 800KB/s speeds using STM32F407's USB FS CDC, which is a bit higher than your estimated 6Mbps.
2019-07-02 9:03 PM
thank you for your comment.
2019-07-04 12:19 AM
hi After Forever and everyone
I want your suggestion.
I connected a laptop (Windows 10) and STM32L4 (60 MHz) with a USB cable.
90 Kbytes of data were sent from the PC to the STM32L4 internal RAM using the USB FS CDC.
The transfer time was 7 seconds.
It is about 103 kbps.
I think it's slow, is it like this?
STM32F7 has faster clock than STM32L4 CPU.
Do you think that the clock speed is fast and the communication speed is fast?