cancel
Showing results for 
Search instead for 
Did you mean: 

Where can I download the workshop package needed to prepare on my side before the session?

Roman LUDIN
ST Employee
 
4 REPLIES 4
Roman LUDIN
ST Employee
MDaub.2
Associate II

I downloaded the material from that Google Drive (SHA1 hash of EXE: 4A657180EB95C812A00ABF43137D1C833296C19D) and I understand according to the setup PDF it should contain all necessary tools like CubeIDE, MX, etc.? But after unpacking/installing it only seemed to have installed the pure workshop material but not the tools? The big Cube Package of 1.1 GB really only seems to be add-on material but not CubeIDE itself? Am I missing a download link? CubeIDE itself is also not available in the public download area in version 1.7. I see the material package has been updated on July, 1st. Was there a problem repackaging maybe so the tools have been left out?

0693W00000BcjA6QAJ.png 

MDaub.2
Associate II

0693W00000BcjAzQAJ.png0693W00000BcjAuQAJ.pngJust noticed there seem to be 2 different Homework PDFs with the same name. The first contains download links to CubeIDE 1.6.1 but the 2nd seems to mention we need 1.7. Which one is the valid one?

MDaub.2
Associate II

Well, seems everything works fine on 1.6.1 a well, so nvm.