cancel
Showing results for 
Search instead for 
Did you mean: 

Virtual COM port in Win7 or Vista 32-bit

bostjan
Associate II
Posted on February 07, 2010 at 21:59

Virtual COM port in Win7 or Vista 32-bit

#stm32 #stm32 #stm32 #lmgtfy #stm32-virtual-com-port-vista-windows-7
22 REPLIES 22
bostjan
Associate II
Posted on May 17, 2011 at 13:39

Hello,

Thank you for your .inf file and the screenshots. I tried the inf file immediatly on my Vista, but the same Code 10 error is happening. Am i doing something wrong wirhin the code ?

I'll try to debug the code and hopefully i find the problem.

Thanks for now,

b
Posted on May 17, 2011 at 13:39

Hi bsmisl,

Here you go : new Driver ''stmcdc.zip'' which contains only one .inf file compliant with all Microsoft Windows Operating system so far including Windows 7 ( either x86 or x64 ).

For full proof, I have attached the Screen shots that show that it is working properly with

Windows 2000

Windows XP

Windows Vista (x86 and x64)

Windows 7 (x86 and x64)

Enjoy it

0690X0000060Ml1QAE.gif

STOne-

Posted on May 17, 2011 at 13:39

Hi ,

You can also

refer to the following article for an explanation of what error code 10 at Microsoft :

Explanation of error codes generated by Device Manager

http://support.microsoft.com/kb/310123

Follow the steps listed for Error Code 10 to see if that helps to resolve your issue or not.

Please post back to let us know if this information was helpful or not so that we may further assist you if need be.

Cheers,

STOne-32.

bostjan
Associate II
Posted on May 17, 2011 at 13:39

Hello,

About the Code 10 error, i found nothing usefull, my device is still not working under Vista or Win7. I think it might be something in the code. I have done some USB sniffing with the SnoopyPRO but i do not know if any thing is wrong. Has any one have the sniffers log, from the Vista or Win7 ?

I hope i find something to fix this.

Thanks,

b

bostjan
Associate II
Posted on May 17, 2011 at 13:39

Good day,

I got it to work on all OS.

The problems were in the buffer sizes, that i fixed and it all works like a charm now.

Well, thank you all for help,

Greets,

b
Posted on May 17, 2011 at 13:39

Well done 0690X0000060Ml2QAE.gif

dimasusl2
Associate
Posted on May 17, 2011 at 13:39

marcomarco9
Associate II
Posted on May 17, 2011 at 13:39

I've the same issue. If I don't set buffer size to 64, I get error 10 in Windows. Is this normal? There's a way to use a greater buffer?

Posted on May 17, 2011 at 13:39

Dear all,

WHQL / Microsoft certified CDC (Serial driver) available on web

We have uploaded a new automatic install of  new certified WHQL driver on Microsoft ( 2000 , XP, Vista and W7 : x86 and x64) : 1.3.1 for CDC driver 

http://www.st.com/stonline/products/support/micro/files/VCP_Setup.zip

It is also available at Windows Update web Site as well.

Cheers,

STOne-32