Posted on May 17, 2011 at 14:04I've used a second buffer more large than 64 bytes.Everytime the usb interrupt occur check if there's a message in the 64bytes buffer.If yes, copy the character received in the second buffer. Next time the usb interrup...
Posted on May 17, 2011 at 13:39I've the same issue. If I don't set buffer size to 64, I get error 10 in Windows. Is this normal? There's a way to use a greater buffer?