USE_HAL_***_REGISTER_CALLBACKS and HAL_SPI_xxxCpltCallback not called
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-01 2:27 AM
After each project update, CubeMX 5x/6x changes the values of all USE_HAL_***_REGISTER_CALLBACKS definitions in stm32h7xx_hal_conf.h header file. This makes it extremely difficult to use the callback functions.
PS:
Hi, today I lost the whole day to find out why the H743 doesn't work
void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi)
and other Callback related SPIs do not work with H743.
This is the function that sends the data but does not call the callback
void test()
{
uint8_t buffer[] = {1,2,3,4};
HAL_SPI_Transmit_IT (&hspi1,buffer, sizeof (buffer) );
}
I want to ask if this is a mistake or has another idea.
at F7xxx it works normally and at the end of the transmission the function is called
SPI_CloseTx_ISR (hspi);
and it is in it that this callback is called.
STM32H7xx_HAL_Driver\Src\stm32h7xx_hal_spi
static void SPI_TxISR_8BIT(SPI_HandleTypeDef hspi)
{
/ Transmit data in 8 Bit mode */
*(__IO uint8_t *)&hspi->Instance->TXDR = *((uint8_t *)hspi->pTxBuffPtr);
hspi->pTxBuffPtr += sizeof(uint8_t);
hspi->TxXferCount--;
/* Disable IT if no more data excepted /
if (hspi->TxXferCount == 0UL)
{
#if defined(USE_SPI_RELOAD_TRANSFER)
/ Check if there is any request to reload /
if (hspi->Reload.Requested == 1UL)
{
hspi->TxXferSize = hspi->Reload.TxXferSize;
hspi->TxXferCount = hspi->Reload.TxXferSize;
hspi->pTxBuffPtr = hspi->Reload.pTxBuffPtr;
}
else
{
/ Disable TXP interrupts /
__HAL_SPI_DISABLE_IT(hspi, SPI_IT_TXP);
}
#else
/ Disable TXP interrupts /
__HAL_SPI_DISABLE_IT(hspi, SPI_IT_TXP);
#endif / USE_HSPI_RELOAD_TRANSFER */
}
}
STM32F7xx_HAL_Driver\Src\stm32f7xx_hal_spi.c
/**
@brief Handle the data 8-bit transmit in Interrupt mode.
@param hspi pointer to a SPI_HandleTypeDef structure that contains
the configuration information for SPI module.
@retval None
*/
static void SPI_TxISR_8BIT(struct __SPI_HandleTypeDef *hspi)
{
*(__IO uint8_t )&hspi->Instance->DR = (hspi->pTxBuffPtr);
hspi->pTxBuffPtr++;
hspi->TxXferCount--;
if (hspi->TxXferCount == 0U)
{
#if (USE_SPI_CRC != 0U)
if (hspi->Init.CRCCalculation == SPI_CRCCALCULATION_ENABLE)
{
/* Enable CRC Transmission /
SET_BIT(hspi->Instance->CR1, SPI_CR1_CRCNEXT);
}
#endif / USE_SPI_CRC */
SPI_CloseTx_ISR(hspi);
}
}
This happens in versions V1.6.0, V1.7.0 and V1.8.0,
/* SPI in mode Transmitter -------------------------------------------------*/
if (HAL_IS_BIT_CLR(trigger, SPI_FLAG_UDR) && HAL_IS_BIT_SET(trigger, SPI_FLAG_TXP) && HAL_IS_BIT_CLR(trigger, SPI_FLAG_DXP))
{
hspi->TxISR(hspi);
handled = 1UL;
}
#if defined(USE_SPI_RELOAD_TRANSFER)
/* SPI Reload -------------------------------------------------*/
if (HAL_IS_BIT_SET(trigger, SPI_FLAG_TSERF))
{
hspi->Reload.Requested = 0UL;
__HAL_SPI_CLEAR_TSERFFLAG(hspi);
}
#endif /* USE_HSPI_RELOAD_TRANSFER */
if (handled != 0UL)
{
return;
}
/* SPI End Of Transfer: DMA or IT based transfer */
if (HAL_IS_BIT_SET(trigger, SPI_FLAG_EOT))
as far as I understand the function is merged into the above function, but `handled` is always `handled = 1UL; `
here is solution from me
/* SPI in mode Transmitter -------------------------------------------------*/
if (HAL_IS_BIT_CLR(trigger, SPI_FLAG_UDR) && HAL_IS_BIT_SET(trigger, SPI_FLAG_TXP) && HAL_IS_BIT_CLR(trigger, SPI_FLAG_DXP))
{
hspi->TxISR(hspi);
// handled = 1 ; //-bobby
handled = hspi->TxXferCount ; //+bobby
}
#if defined(USE_SPI_RELOAD_TRANSFER)
/* SPI Reload -------------------------------------------------*/
if (HAL_IS_BIT_SET(trigger, SPI_FLAG_TSERF))
{
hspi->Reload.Requested = 0UL;
__HAL_SPI_CLEAR_TSERFFLAG(hspi);
}
#endif /* USE_HSPI_RELOAD_TRANSFER */
if (handled != 0UL)
{
return;
}
/* SPI End Of Transfer: DMA or IT based transfer */
// if (HAL_IS_BIT_SET(trigger, SPI_FLAG_EOT)) // -bobby
if ((HAL_IS_BIT_SET(trigger, SPI_FLAG_EOT))||(HAL_IS_BIT_SET(hspi->Instance->SR, SPI_FLAG_TXTF))) //+bobby
{
/* Clear EOT/TXTF/SUSP flag */
__HAL_SPI_CLEAR_EOTFLAG(hspi);
__HAL_SPI_CLEAR_TXTFFLAG(hspi);
__HAL_SPI_CLEAR_SUSPFLAG(hspi);