2024-03-26 09:57 AM - edited 2024-03-26 10:13 AM
Hello Everybody,
I use STM32CubeIDE1.15.0 Build: 20695_20240315_1429 and a custom board with a STM32303RE inside.
I use the IOC interface to set the virtual port com. Everything work fine, just a detail: when i connect, then disconnect and reconnect the USB port, the port com number on Windows change, It increase (search the next available number)! The VID and PID are always the same, so I focus on the serial number, and i found that (code generate by STM32CubeIde):
😉
)
2024-03-26 10:17 AM - edited 2024-03-26 10:20 AM
Just a bug. Consistent serial numbers can be created from anything else, for example programmed in OTP flash or eeprom.