2019-12-08 9:59 AM
Hello,
I've been using the NUCLEO-L476RG board for development. Now I want to design my own PCB with the same component. My question is about the JTAG port - in the NUCLEO board it is implemented as a USB connector but they used an additional uC for that. I would like to use only the stm32l476RG. I see in its datasheet that it has USB connectivity but I can't find the USB pins in the pinout section.
Would appreciate some kind of reference or application notes for USB connector for this coponent, so that I'll be able to connect it to a PC in order to program it, debug and read data over serial.
Thank you,
David
Solved! Go to Solution.
2019-12-08 10:29 PM
Thanks a lot!