User Activity

Hello,I'm using NUCLEO-L476RG connected to eval board of LSM6DSL. I have checked the physical connection with a DVM and it seems to be correct.I have generated a very simple project using STM32CubeIDE and trying to read the WHO_AM_I register (code be...
Hello,I'm designing a custom PCB with STM32L476RG. I need to add Bluetooth 5 connectivity. I'm looking for a BT module with the following requirements:Transmit at least 2MbpsAs small as possibleIt would be great if it will come with code exampleI don...
Hello,I've been using the NUCLEO-L476RG board for development. Now I want to design my own PCB with the same component. My question is about the JTAG port - in the NUCLEO board it is implemented as a USB connector but they used an additional uC for t...